43.3.4.8 Compare
Purpose
The purpose of this service is to compare two numbers in classical arithmetic GF(p).
How to Use the Service
Description
This service accepts two numbers in classical arithmetic in input and performs a comparison, virtually subtracting (X + CarryIn) from Y:
CompareGetFlags (Y - (X + CarryIn))
The numbers X and Y are untouched but the resulting flags CarryOut and the Zero Bit are filled. If the lengths of Y and X are equal, a comparison is processed.
If the length of Y is strictly greater than the length of X, X is first virtually padded with zeros on the Most Significant Bytes side, then a comparison is processed.
In this computation, the following data need to be provided:
- X (pointed by{nu1XBase,u2XLength})
- Y (pointed by{nu1YBase,u2YLength})
The service name for this operation is
Comp.
Parameters Definition
| Parameter | Type | Direction | Location | Data Length | Before Executing the Service | After Executing the Service |
|---|---|---|---|---|---|---|
| Specific/Gf2n CarryIn | Bits | I | – | – | GF(2n) Bit and Carry In | – |
| Specific/CarryOut Zero Violation | Bits | I | – | – | – | Carry Out, Zero Bit and Violation Bit filled according to the result |
| nu1XBase | nu1 | I | Crypto RAM | u2XLength | Base of X | Base of X |
| u2XLength | u2 | I | – | – | Length of X | Length of X |
| nu1YBase | nu1 | I | Crypto RAM | u2YLength | Base of Y | Base of Y |
| u2YLength | u2 | I | – | – | Length of Y | Length of Y |
Code Example
PUKCL_PARAM PUKCLParam;
PPUKCL_PARAM pvPUKCLParam = &PUKCLParam;
// CarryIn shall be beforehand filled (with zero or one) PUKCL(Specific).CarryIn = ...;
// Initializing parameters
PUKCL_Comp(nu1XBase) = <Base of the ram location of X>;
PUKCL_Comp(u2XLength) = <Length of X>;
PUKCL_Comp(nu1YBase) = <Base of the ram location of Y>;
PUKCL_Comp(u2YLength) = <Length of Y>;
// vPUKCL_Process() is a macro command,
// and then calls the library...
vPUKCL_Process(Comp,pvPUKCLParam);
if (PUKCL(u2Status) == PUKCL_OK)
{
// The COMPARE has been executed correctly
// CarryOut, Zero ... are available
... = PUKCL(Specific).CarryOut;
... = PUKCL(Specific).Zero;
}
else // Manage the error
Constraints
The following conditions must be avoided to ensure that the service works correctly:
- nu1XBase or nu1YBase are not aligned on 32-bit boundaries
- {nu1XBase, u2XLength} or {nu1YLength, u2YLength} are not in Crypto RAM
- u2XLength or u2YLength is either: < 4, > 0xffc or not a 32-bit length or u2XLength >u2YLength
Status Returned Values
| Returned Status | Importance | Meaning |
|---|---|---|
| PUKCL_OK | – | Service functioned correctly |