43.3.4.1 SelfTest
Purpose
This service is used to initialize the PUKCL. It resets the PUKCC, clears the Crypto RAM, and returns the library and PUKCC version numbers.
It must be called before using any other services in the library and the user must verify the return status at the end of the service execution.
How to Use the Service
Description
This service processes internal tests and returns
information and status codes as described in Status Returned Values. The service name for this
operation is SelfTest.
Parameters Definition
It is possible to directly address this service
through the PUKCL_SelfTest() macro.
| Parameter | Type | Dir. | Location | Data Length | Before Executing the Service | After Executing the Service |
|---|---|---|---|---|---|---|
| u4Version | u4 | O | – | – | – | PUKCL version |
| u4PUKCCVersion | u4 | O | – | – | – | PUKCC Version |
| u4CheckNum1 | u4 | O | – | – | – | Test result value 1 |
| u4CheckNum2 | u4 | O | – | – | – | Test result value 2 |
| u1Step | u1 | O | – | – | – | Latest correctly executed step |
Code Example
PUKCL_PARAM PUKCLParam;
PPUKCL_PARAM pvPUKCLParam = &PUKCLParam;
// vPUKCL_Process() is a macro command, which populates the service name
// and then calls the library
vPUKCL_Process(SelfTest,pvPUKCLParam);
if (PUKCL(u2Status) == PUKCL_OK)
{
// The Library version is available
// in PUKCL_SelfTest(u4Version)
// The PUKCL version is available
// in PUKCL_SelfTest(u4PUKCCVersion)
}
Returned Values
The expected u4Version value depends on the version of PUKCL being used, and the u4PUKCCVersion value depends on the version of PUKCC being used.
The expected u4CheckNum1 value is 0x6e70ddd2 and the expected one for u4CheckNum2 is 0x25c8d64f. The expected final u1Step value is 3.
Status Returned Values
| Returned Status | Importance | Meaning |
|---|---|---|
| PUKCL_OK | – | Service functioned correctly. |
| PUKCL_ERROR | Severe | An issue has been encountered. |