2.2.4.34 USB_DEVICE_CONTROL_STATUS Enumeration

C

typedef enum {
  USB_DEVICE_CONTROL_STATUS_OK,
  USB_DEVICE_CONTROL_STATUS_ERROR
} USB_DEVICE_CONTROL_STATUS;

Summary

Control Transfer Status Stage Flags

This enumeration defines the flags to be used with the USB_DEVICE_ControlStatus function.

Members

Members Description
USB_DEVICE_CONTROL_STATUS_OK Using this flag acknowledges the Control transfer. A Zero Length Packet will be transmitted in the status stage of the control transfer.
USB_DEVICE_CONTROL_STATUS_ERROR Using this flag stalls the control transfer. This flags should be used if the control transfer request needs to be declined.