3.3.4.34 USB_HOST_AUDIO_V1_StreamingInterfaceSet Function
C
USB_HOST_AUDIO_V1_RESULT USB_HOST_AUDIO_V1_StreamingInterfaceSet(
USB_HOST_AUDIO_V1_STREAM_HANDLE streamHandle,
USB_HOST_AUDIO_V1_REQUEST_HANDLE * requestHandle,
USB_HOST_AUDIO_V1_STREAMING_INTERFACE_SETTING_OBJ interfaceSettingObj
);
Summary
This function schedules an audio stream enable request for the specified audio stream. An audio stream must be enable before scheduling any data transfer with the stream. A USB_HOST_AUDIO_V1_STREAM_EVENT_ENABLE_COMPLETE event is generated when this request is completed. USB_HOST_AUDIO_V1_STREAM_EVENT_ENABLE_COMPLETE_DATA returns the status and request handle of the request.
Precondition
The audio stream should have been opened. Only one audio stream from an audio stream group can be enabled at a time.
Parameters
| Parameters | Description |
| streamHandle | Handle to the Audio v1.0 stream. |
| requestHandle | Handle to the stream enable request. |
| interfaceSettingObj | Audio streaming interface setting object. |
Returns
- USB_HOST_AUDIO_V1_RESULT_SUCCESS - The operation was successful
- USB_HOST_AUDIO_V1_RESULT_HANDLE_INVALID - The specified audio stream does not exist
- USB_HOST_AUDIO_V1_RESULT_FAILURE - An unknown failure occurred
Remarks
None.