3.3.4.1 USB_HOST_AUDIO_V1_AttachEventHandlerSet Function
C
USB_HOST_AUDIO_V1_RESULT USB_HOST_AUDIO_V1_AttachEventHandlerSet(
USB_HOST_AUDIO_V1_ATTACH_EVENT_HANDLER eventHandler,
uintptr_t context
);
Summary
This function will set an attach event handler. The attach event handler will be called when a Audio v1.0 Device has been attached or detached. The context will be returned in the event handler. This function should be called before the bus has been enabled.
Parameters
| Parameters | Description |
| eventHandler | Pointer to the attach event handler. |
| context | An application defined context that will be returned in the event handler. |
Returns
- USB_HOST_AUDIO_V1_RESULT_SUCCESS - If the attach event handler was registered successfully
- USB_HOST_AUDIO_V1_RESULT_FAILURE - If the number of registered event handlers has exceeded USB_HOST_AUDIO_V1_ATTACH_LISTENERS_NUMBER
Remarks
This function should be called before the USB_HOST_BusEnable function is called.