3.3.4.42 USB_HOST_AUDIO_V1_StreamSamplingFrequencySet Function
C
USB_HOST_AUDIO_V1_RESULT USB_HOST_AUDIO_V1_StreamSamplingFrequencySet(
USB_HOST_AUDIO_V1_STREAM_HANDLE streamHandle,
USB_HOST_AUDIO_V1_REQUEST_HANDLE * requestHandle,
const uint32_t * samplingFrequency
);
Summary
This function schedules an audio stream set sampling rate request for the specified audio stream. A USB_HOST_AUDIO_V1_STREAM_EVENT_SAMPLING_RATE_SET_COMPLETE event is generated when this request is completed. USB_HOST_AUDIO_V1_STREAM_EVENT_SAMPLING_RATE_SET_COMPLETE_DATA returns the status and request handle of the request.
Precondition
The audio stream should have been opened.
Parameters
| Parameters | Description |
| streamHandle | Handle to the Audio v1.0 stream |
| requestHandle | Handle to the stream set sampling rate request |
| samplingFrequency | Pointer to the sampling rate |
Returns
- USB_HOST_AUDIO_V1_RESULT_SUCCESS - The operation was successful
- USB_HOST_AUDIO_V1_RESULT_HANDLE_INVALID - The specified audio stream does not exist
- USB_HOST_AUDIO_V1_RESULT_FAILURE - An unknown failure occurred
Remarks
None.