3.5.2 Using the Library
This topic describes the basic architecture of the USB HID Host Mouse Driver Library and provides information and examples on its use.
Topics
| Name | Description | 
| Abstraction Model | Describes the Abstraction Model of the USB HID Host Mouse Driver Library. | 
| Library Overview | The USB HID Host Mouse Driver can be grouped functionally as shown in the following table. | 
| How the Library Works | Describes how the library works and how it should be used. |