3.2.6 PIO Branching Structure
Most PIO lines share multiple functions and are branched to multiple destinations through passive resistors on the SAMA7G54 Curiosity Pro board.
In the above example, FLEXCOM11_IO0 is branched to two MOSI signal paths through separate series resistors.
In some application-specific contexts, such MOSI lines can also be connected to signals other than SPI MOSI nets. This is especially common for signals originating from extension connectors such as mikroBUS1 and mikroBUS2.
Because two connected devices cannot drive the line at the same time, some arbitration is required. The user must ensure that the software application manages the situation correctly by enabling only one device at a time or by setting up the system hardware to prevent conflicts. This can be achieved by disconnecting some devices from the line at the other end or by removing the corresponding series resistors (R74 and R75 in this example).
The schematic and tables below summarize the overall PIO branching structure on the SAMA7G54 Curiosity Pro board to help visualize the connections and resistors present on each PIO path.
- Empty cells (–) in the two
leftmost columns indicate that one SAM PIO/signal is directed to multiple end
destinations.
Example: PA10 connects to three destinations via three intermediary resistors.
- Empty cells (–) in the two
rightmost columns indicate that the SAM PIO/signal connects directly to the end
destination, without an intermediary resistor.
Example: PA00/SDMMC0_CLK and PA01/SDMMC0_CMD connect directly to the SD card.
| PIO Line | Net at SAMA7G54 Pin | Resistor | Net after the Resistor |
|---|---|---|---|
PA00 | SDMMC0_CLK | – | – |
PA01 | SDMMC0_CMD | – | – |
PA02 | M2_WIFI_NRST | – | – |
PA03 | SDMMC0_DATA0 | – | – |
PA04 | SDMMC0_DATA1 | – | – |
PA05 | SDMMC0_DATA2 | – | – |
PA06 | SDMMC0_DATA3 | – | – |
PA07 | PA07_MUX | R35 | MBUS0_TX |
| – | – | R361 | CAN1_TX |
PA08 | PA08_MUX | R45 | MBUS0_RX |
| – | – | R461 | CAN1_RX |
PA09 | PA09_MUX | R31 | RPI_GPIO27 |
| – | – | R321 | CAN0_TX |
PA10 | PA10_MUX | R341 | CAN0_RX |
| – | PA10_MUX | R33 | FLEXCOM5_IO0 |
| – | FLEXCOM5_IO0 | R48 | ISC_TWD |
| – | – | R125 | MIPI_TWD |
| – | – | R126 | MBUS0_TWD |
| – | – | R127 | MBUS1_TWD |
| – | – | R128 | RPI_TWD |
| – | – | R50 | M2_WIFI_TWD |
PA11 | FLEXCOM5_IO1 | R40 | ISC_TWCK |
| – | – | R114 | MIPI_TWCK |
| – | – | R115 | MBUS0_TWCK |
| – | – | R116 | MBUS1_TWCK |
| – | – | R118 | RPI_TWCK |
| – | – | R49 | M2_WIFI_TWCK |
PA12 | M2_WIFI_WAKE | – | – |
PA13 | RPI_GPIO23 | – | – |
PA14 | PAC1934_nINT | – | – |
PA15 | GMAC0_TXEN | – | – |
PA16 | GMAC0_TX0 | – | – |
PA17 | GMAC0_TX1 | – | – |
PA18 | GMAC0_RXCTL | – | – |
PA19 | GMAC0_RX0 | – | – |
PA20 | GMAC0_RX1 | – | – |
PA21 | RPI_GPIO24 | – | – |
PA22 | GMAC0_MDC | – | – |
PA23 | GMAC0_MDIO | – | – |
PA24 | GMAC0_TXCK | – | – |
PA25 | M2_WIFI_IRQ | – | – |
PA26 | GMAC0_TX2 | – | – |
PA27 | GMAC0_TX3 | – | – |
PA28 | GMAC0_RX2 | – | – |
PA29 | GMAC0_RX3 | – | – |
PA30 | GMAC0_RXCK | – | – |
PA31 | M2_WIFI_TW_IRQ | – | – |
PB00 | MIPI_ENABLE | – | – |
PB01 | GMAC1_INT | – | – |
PB02 | RPI_GPIO22 | – | – |
PB03 | FLEXCOM11_IO0 | R74 | MBUS0_MOSI |
| – | – | R75 | MBUS1_MOSI |
PB04 | FLEXCOM11_IO1 | R79 | MBUS0_MISO |
| – | – | R80 | MBUS1_MISO |
PB05 | FLEXCOM11_IO2 | R84 | MBUS0_SCK |
| – | – | R85 | MBUS1_SCK |
PB06 | FLEXCOM11_IO3 | R89 | MBUS0_CS |
PB07 | FLEXCOM11_IO4 | R91 | MBUS1_CS |
PB08 | FLEXCOM8_IO0 | R42 | RPI_MOSI |
| – | – | R43 | GMAC0_MOSI |
PB09 | FLEXCOM8_IO1 | R44 | RPI_MISO |
| – | – | R47 | GMAC0_MISO |
PB10 | FLEXCOM8_IO2 | R51 | RPI_SCK |
| – | – | R52 | GMAC0_SCK |
PB11 | FLEXCOM8_IO3 | R53 | RPI_NPCS0 |
PB12 | FLEXCOM8_IO4 | R55 | RPI_NPCS1 |
| – | – | R56 | GMAC0_CS |
PB13 | M2_BT_TX | – | – |
PB14 | M2_BT_RX | – | – |
PB15 | LED_BLUE | – | – |
PB16 | M2_BT_CTS | – | – |
PB17 | M2_BT_RTS | – | – |
PB18 | RPI_GPCLK1 | – | – |
PB19 | RPI_GPCLK2 | – | – |
PB20 | MIPI_IRQ | – | – |
PB21 | PB21_MUX | R14 | MBUS0_nRST |
| – | – | R38 | MBUS1_nRST |
| – | – | R39 | RPI_GPIO25 |
PB22 | QSPI1_IO3 | – | – |
PB23 | QSPI1_IO2 | – | – |
PB24 | QSPI1_IO1 | – | – |
PB25 | QSPI1_IO0 | – | – |
PB26 | QSPI1_CS | – | – |
PB27 | QSPI1_SCK | – | – |
PB28 | USBIO_INT_A | – | – |
PB29 | SDMMC1_CMD | – | – |
PB30 | SDMMC1_CLK | – | – |
PB31 | SDMMC1_DATA0 | – | – |
PC00 | SDMMC1_DATA1 | – | – |
PC01 | SDMMC1_DATA2 | – | – |
PC02 | SDMMC1_DATA3 | – | – |
PC03 | MBUS0_INT | – | – |
PC04 | SDMMC1_CD | – | – |
PC05 | PC5_MUX | R76 | ISC_PWDN |
| – | – | R77 | SDMMC1_1V8SEL |
PC06 | USBIO_VBDET_A | – | – |
PC07 | RPI_TXD | – | – |
PC08 | RPI_RXD | – | – |
PC09 | MBUS1_TX | – | – |
PC10 | MBUS1_RX | – | – |
PC11 | RPI_I2S_CK | – | – |
PC12 | RPI_I2S_WS | – | – |
PC13 | MBUS1_AN | – | – |
PC14 | RPI_I2S_DOUT0 | – | – |
PC15 | MBUS0_AN | – | – |
PC16 | MBUS1_INT | – | – |
PC17 | GMAC0_INT | – | – |
PC18 | RPI_I2S_DIN0 | – | – |
PC19 | PMIC_nINT | – | – |
PC20 | RPI_GPIO26 | – | – |
PC21 | NAND_DAT3 | – | – |
PC22 | NAND_DAT4 | – | – |
PC23 | NAND_DAT5 | – | – |
PC24 | NAND_DAT6 | – | – |
PC25 | JTAG_NRST | – | – |
PC26 | JTAG_TCK | – | – |
PC27 | JTAG_TMS | – | – |
PC28 | JTAG_TDI | – | – |
PC29 | JTAG_TDO | – | – |
PC30 | FLEXCOM10_IO0 | R106 | PMIC_TWD |
| – | – | R107 | PAC1934_TWD0 |
| – | – | R108 | EEPROM_TWD |
| – | – | R109 | GMAC0_TWD |
PC31 | FLEXCOM10_IO1 | R100 | PMIC_TWCK |
| – | – | R101 | PAC1934_TWCK0 |
| – | – | R103 | EEPROM_TWCK |
| – | – | R104 | GMAC0_TWCK |
PD00 | RPI_GPIO16 | – | – |
PD01 | RPI_GPIO17 | – | – |
PD02 | NAND_DAT7 | – | – |
PD03 | NAND_RDY | – | – |
PD04 | NAND_CS | – | – |
PD05 | NAND_WE | – | – |
PD06 | NAND_OE | – | – |
PD07 | NAND_ALE | – | – |
PD08 | NAND_CLE | – | – |
PD09 | NAND_DAT0 | – | – |
PD10 | NAND_DAT1 | – | – |
PD11 | NAND_DAT2 | – | – |
PD12 | RPI_GPCLK0 | – | – |
PD13 | LED_RED | – | – |
PD14 | LED_GREEN | – | – |
PD15 | PD15_MUX | R57 | MBUS0_PWM |
| – | – | R58 | MBUS1_PWM |
PD16 | PD16_MUX | R64 | DBGU_TX |
| – | – | R651 | CAN2_TX |
PD17 | PD17_MUX | R72 | DBGU_RX |
| – | – | R731 | CAN2_RX |
PD18 | RPI_PWM1 | – | – |
PD19 | USER_BUTTON | – | – |
PD20 | RPI_PWM0 | – | – |
PD21 | GMAC1_TXEN | – | – |
PD22 | GMAC1_TX0 | – | – |
PD23 | PD23_PP | J5 | ISC_MCK |
| – | – | – | GMAC1_TX1 |
PD24 | PD24_PP | J6 | ISC_D0 |
| – | – | – | GMAC1_CRSDV |
PD25 | PD25_PP | J7 | ISC_D1 |
| – | – | – | GMAC1_RX0 |
PD26 | PD26_PP | J8 | ISC_D2 |
| – | – | – | GMAC1_RX1 |
PD27 | PD27_PP | J9 | ISC_D3 |
| – | – | – | GMAC1_RXER |
PD28 | PD28_PP | J10 | ISC_D4 |
| – | – | – | GMAC1_MDC |
PD29 | PD29_PP | J11 | ISC_D5 |
| – | – | – | GMAC1_MDIO |
PD30 | PD30_PP | J12 | ISC_D6 |
| – | – | – | GMAC1_REFCLK |
PD31 | PD31_PP | J13 | ISC_D7 |
| –– | – | – | USBIO_OC_B |
PE00 | PE0_PP | J14 | ISC_HSYNC |
| – | – | – | USBIO_OC_C |
PE01 | PE01_PP | J15 | ISC_VSYNC |
| – | – | – | USBIO_EN_B |
PE02 | PE02_PP | J16 | ISC_PWR_EN |
| – | – | – | USBIO_EN_C |
PE03 | PE03_PP | J17 | ISC_PCK |
| – | – | – | FLEXCOM0_IO0 |
| – | FLEXCOM0_IO0 | R60 | M2_WIFI_MOSI |
| – | – | R61 | USBIO_SPI_MOSI_A |
PE04 | PE04_PP | J18 | ISC_D8 |
| – | – | – | FLEXCOM0_IO1 |
| – | FLEXCOM0_IO1 | R62 | M2_WIFI_MISO |
| – | – | R63 | USBIO_SPI_MISO_A |
PE05 | PE05_PP | J19 | ISC_D9 |
| – | – | – | FLEXCOM0_IO2 |
| – | FLEXCOM0_IO2 | R66 | M2_WIFI_SCK |
| – | – | R67 | USBIO_SPI_SCK_A |
PE06 | PE06_PP | J20 | ISC_D10 |
| – | – | – | FLEXCOM0_IO3 |
| – | FLEXCOM0_IO3 | R68 | M2_WIFI_CS |
PE07 | PE07_PP | J21 | ISC_D11 |
| – | – | – | FLEXCOM0_IO4 |
| FLEXCOM0_IO4 | R70 | USBIO_SPI_CS_A |
- Not populated.