15.1.2.8 WRERR Bit
The WRERR bit can be used to determine if a write error occurred. WRERR will be
set if one of the following conditions occurs:
- If WR is set while the NVMADRH:NMVADRL points to a write-protected address
- A Reset occurs while a self-write operation was in progress
- An unlock sequence was interrupted
The WRERR bit is normally set by hardware, but can be set by the user for test purposes. Once set, WRERR must be cleared in software.
Free | LWLO | Actions for PFM when WR =
1 |
Comments |
---|---|---|---|
1 |
x | Erase the 32-word row of NVMADRH:NVMADRL location. |
|
0 |
1 |
Copy NVMDATH:NVMDATL to the write latch corresponding to NVMADR LSBs. |
|
0 |
0 |
Write the write-latch data to PFM row. |
|