The purpose of fastPollingMode is to continuously check all participating service/channel configurations for valid telegrams without any interruption. This mode is very similar to the PollingMode but there is no support of the self-check functionality and no sleep period is executed (see the following figure). Fast polling is also known as scanning.Figure 3-15. Fast Polling Cycle Definition
If the polling period is set to 0 ms in the confT1COR EEPROM setting, fastPollingMode is
activated. During operation, fastPollingMode can be enabled by overwriting the confT1COR
SRAM variable manually with 0x00 by using the “Write SRAM/Register” SPI command if the
system is in IDLEMode. See Write SRAM/Register from Related Links.
Note: EOP signals are ignored in this mode.
Furthermore, VCO tuning on the initial service/channel configuration is not supported.
See VCO Tuning from Related Links.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.