4.1 Getting Started with MCHPRT3 Tool GUI for the WILCS02_WINCS02
The following are the steps to launch the MCHPRT3 tool:
- Double click the
MCHPRT3.exefile to launch the MCHPRT3 tool. - From the “Select GUI” drop-down list, select WILCS02_WINCS02.
- Click Open to launch the WILCS02_WINCS02 window (see the following
figure).
Figure 4-2. Start-Up Window of the MCHPRT3 Tool - The WILCS02_WINCS02 window is divided into the following sections (see the
following figure):
- RF tab: Provides settings to perform the RF TX Modulation, TX Tone, RX Test
- Calibration tab: Complete TX and RX Calibration flow
- MAC Address tab: Read/Write Wi-Fi® Address
- Gain Tables tab: Process Gain Table relate function
- Misc. tab: Process
others, example Post Cal
Figure 4-3. Start-up Window of the WILCS02_WINCS02 GUI Tool