In this demonstration, the user can receive Wi-Fi® packets on the WILCS02_WINCS02. perform the following step for receiving
Wi-Fi Packets.Figure 4-8. RF RX Test
Demonstration
In the RF tab, perform the following steps:
From the “Channel” drop-down list, select 2442
MHz for channel 7.
From the “Rate Type” drop-down list, select
Legacy for 11b and 11g Mode, MCS for 11n mode or ALL –
RX Only for all data rates.
From the “Data Rate” drop-down list, select 1
Mbps – 11b for 11b Mode and 1 Mbps.
In the RX tab, perform the following steps:
Click Start RX to receive Wi-Fi packets as
configured in step 1. Use IQxel Wi-Fi tester or other tools to send the
Wi-Fi packets to the WILCS02_WINCS02
device.
Click Stop RX to stop receiving the Wi-Fi
packets.
Click Get RX Count. The “RX Count Information” table shows the received Wi-Fi packets.
Click Clear RX Count to Reset RX Count
Information.
Repeat the above steps for a new RX test.
Click Get RSSI to read the RSSI
value.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.