4.7 MAC Address Programming
In this demonstration, set the MAC address of the Wi-Fi® interfaces
of the WILCS02_WINCS02. In the MAC Address tab,
perform the following steps for MAC Address programming:
- Click the Read Wi-Fi Address button to read the Wi-Fi address.
- Enter the Wi-Fi address to write the Wi-Fi address, for example,
12:34:56:78:9A:BC, then click the Write Wi-Fi Address button.Figure 4-58. MAC Address Programming