4.4 RF TX Tone Test Demonstration
In this demonstration, the user can transmit single tone on the WILCS02_WINCS02. Perform the following steps for the demonstration of the transmission:
- In the RF tab, from the “Channel” drop-down list, select 2442 MHz for channel 7.
- In the TX Tone tab, select gain index from 0 to 255.
- Click Start Tone to transmit single tone as configured in step 1 and 2. Use the Wi-Fi® tester to verify the transmitting single tone.
- Click Stop Tone to stop the
transmission.
Figure 4-7. RF TX Tone Test Demonstration