Enter the “Timeout” value as 5000 (default value)
and click SetTimeout
Note: This value must be greater than 5000
milliseconds.
Check the “Wai Boot Finish” when powering ON the
WILCS02_WINCS02 before pressing the “Connect” button. By
default, the “Wai Boot Finish” is disabled.
Note: The time between powering ON and pressing
the “Connect” button must be shorter than the WILCS02_WINCS02 boot sequence time.
Check the “Temperature Compensation” field if the
test temperature is not at room temperature. By default, the Temperature Compensation is
disabled.
Click Connect to connect the UART of the
WILCS02_WINCS02 (see the following figure).Figure 4-4. Connect Device
Click OK in the pop-up window to Reset the
WILCS02_WINCS02 device. The firmware version appears
instantly (see the following figure).Figure 4-5. Firmware Version
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.