6.3.13 tolower Function
Convert a character to a lowercase alphabetical character.
Include
<ctype.h>
Prototype
int tolower (int c);
Argument
c- The character to convert to lowercase.
Return Value
Returns the corresponding lowercase alphabetical character if the argument,
c, was originally uppercase; otherwise, returns the original
character.
Remarks
Only uppercase alphabetical characters may be converted to lowercase.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <ctype.h>
#include <stdio.h>
int main(void)
{
int ch;
ch = 'B';
printf("B changes to lowercase %c\n",
tolower(ch));
ch = 'b';
printf("b remains lowercase %c\n",
tolower(ch));
ch = '@';
printf("@ has no lowercase, ");
printf("so %c is returned\n", tolower(ch));
}
Example Output
B changes to lowercase b
b remains lowercase b
@ has no lowercase, so @ is returned