6.3.9 ispunct Function
Test for a punctuation character.
Include
<ctype.h>
Prototype
int ispunct (int c);
Argument
c- The character to test.
Return Value
Returns a non-zero integer value if the character, c, is a
punctuation character; otherwise, returns zero.
Remarks
A character is considered to be a punctuation character if it is a printable character
which is neither a space nor an alphanumeric character. Punctuation characters consist
of the
following:
'!' '"' '#' '$' '%' '&' ''' '(' ')' '*' '+' ',' '-' '.' '/' ':'
';' '<' '=' '>' '?' '@' '[' '\' ']' '^' '_' '`' '{' '|' '}' '~'Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <ctype.h>
#include <stdio.h>
int main(void)
{
int ch;
ch = '&';
if (ispunct(ch))
printf("& is a punctuation character\n");
else
printf("& is NOT a punctuation character\n");
ch = '\t';
if (ispunct(ch))
printf("A tab is a punctuation character\n");
else
printf("A tab is NOT a punctuation character\n");
}
Example Output
& is a punctuation character
A tab is NOT a punctuation character