6.3.6 isgraph Function
Test for a graphical character.
Include
<ctype.h>
Prototype
int isgraph (int c);
Argument
c- The character to test.
Return Value
Returns a non-zero integer value if the character, c, is a
graphical character; otherwise, returns zero.
Remarks
A character is considered to be a graphical character if it is any printable character except a space.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <ctype.h>
#include <stdio.h>
int main(void)
{
int ch;
ch = '3';
if (isgraph(ch))
printf("3 is a graphical character\n");
else
printf("3 is NOT a graphical character\n");
ch = '#';
if (isgraph(ch))
printf("# is a graphical character\n");
else
printf("# is NOT a graphical character\n");
ch = ' ';
if (isgraph(ch))
printf("A space is a graphical character\n");
else
printf("A space is NOT a graphical character\n");
}
Example Output
3 is a graphical character
# is a graphical character
A space is NOT a graphical character