6.3.8 isprint Function
Test for a printable character (includes a space).
Include
<ctype.h>
Prototype
int isprint(int c);
Argument
c- The character to test.
Return Value
Returns a non-zero integer value if the character, c, is
printable; otherwise, returns zero.
Remarks
A character is considered to be a printable character if its ASCII value is in the range 0x20 to 0x7e inclusive.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <ctype.h>
#include <stdio.h>
int main(void)
{
int ch;
ch = '&';
if (isprint(ch))
printf("& is a printable character\n");
else
printf("& is NOT a printable character\n");
ch = '\t';
if (isprint(ch))
printf("A tab is a printable character\n");
else
printf("A tab is NOT a printable character\n");
}
Example Output
& is a printable character
A tab is NOT a printable character