6.3.14 toupper Function
Convert a character to an uppercase alphabetical character.
Include
<ctype.h>
Prototype
int toupper (int c);
Argument
c- The character to convert to uppercase.
Return Value
Returns the corresponding uppercase alphabetical character if the argument,
c, was originally lowercase; otherwise, returns the original
character.
Remarks
Only lowercase alphabetical characters may be converted to uppercase.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <ctype.h>
#include <stdio.h>
int main(void)
{
int ch;
ch = 'b';
printf("b changes to uppercase %c\n",
toupper(ch));
ch = 'B';
printf("B remains uppercase %c\n",
toupper(ch));
ch = '@';
printf("@ has no uppercase, ");
printf("so %c is returned\n", toupper(ch));
}
Example Output
b changes to uppercase B
B remains uppercase B
@ has no uppercase, so @ is returned