6.3.11 isupper Function
Test for an uppercase letter.
Include
<ctype.h>
Prototype
int isupper (int c);
Argument
c- The character to test.
Return Value
Returns a non-zero integer value if the character, c, is an
uppercase alphabetic character; otherwise, returns zero.
Remarks
A character is considered to be an uppercase alphabetic character if it is in the range
of 'A'-'Z'.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <ctype.h>
#include <stdio.h>
int main(void)
{
int ch;
ch = 'B';
if (isupper(ch))
printf("B is uppercase\n");
else
printf("B is NOT uppercase\n");
ch = 'b';
if (isupper(ch))
printf("b is uppercase\n");
else
printf("b is NOT uppercase\n");
}
Example Output
B is uppercase
b is NOT uppercase