6.3.4 iscntrl Function
Test for a control character.
Include
<ctype.h>
Prototype
int iscntrl(int c);
Argument
c- The character to test.
Return Value
Returns a non-zero integer value if the character, c, is a
control character; otherwise, returns zero.
Remarks
A character is considered to be a control character if its ASCII value is in the range 0x00 to 0x1F inclusive, or 0x7F.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <ctype.h>
#include <stdio.h>
int main(void)
{
char ch;
ch = 'B';
if (iscntrl(ch))
printf("B is a control character\n");
else
printf("B is NOT a control character\n");
ch = '\t';
if (iscntrl(ch))
printf("A tab is a control character\n");
else
printf("A tab is NOT a control character\n");
}
Example Output
B is NOT a control character
A tab is a control character