6.3.2 isalpha Function
Test for an alphabetic character.
Include
<ctype.h>
Prototype
int isalpha(int c);
Argument
c- The character to test.
Return Value
Returns a non-zero integer value if the character is alphabetic; otherwise, returns zero.
Remarks
Alphabetic characters are included within the ranges
'A'-'Z' or 'a'-'z'.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <ctype.h>
#include <stdio.h>
int main(void)
{
int ch;
ch = 'B';
if (isalpha(ch))
printf("B is alphabetic\n");
else
printf("B is NOT alphabetic\n");
ch = '#';
if (isalpha(ch))
printf("# is alphabetic\n");
else
printf("# is NOT alphabetic\n");
}
Example Output
B is alphabetic
# is NOT alphabetic