3.21.1 Aging Configuration
By default, dynamic entries are removed from the Mac table after 300 seconds. This process is called aging. Aging time can be configured to be in the range of 10 to 1000000 seconds or 0 to disable automatic aging.
Command Syntax:
mac address-table aging-time <v_0_10_to_1000000>Argument | Description | |
Parameter |
| Aging time in seconds, 0 to disable aging. |
Default | Aging time is 300 seconds | |
Mode | Global Configuration mode | |
Usage | Set MAC address table aging time in seconds. To reset to default (300 seconds), use the ‘no’ version of the command. | |
Example | Example 1: Set aging time to 400 seconds. Example 2: Disable automatic aging. | |