3.17.1.3 IGMP Snooping Port Filtering Profile Configuration

Use this command to select the IPMC Profile as the filtering condition for the specific port.

Command Syntax:

ip igmp snooping filter <profile_name>
Table 3-79. Command Description

Argument

Description

Parameter

<profile_name>

Profile name in 16 characters

Default

N.A

Mode

Port List Interface mode

Usage

Select the IPMC Profile as the filtering condition.

Example

Example 1:

Select the testprofile for port 2.

# configure terminal
(config)# interface GigabithEthernet 1/2
(config-if)# ip igmp snooping filter testprofile