3.25.1 MAC-Based VLAN Membership Configuration
Use this command to configure MAC address to VLAN ID mappings. Add/delete MAC-based VLAN Classification List entries and assign the entries to different ports.
Command Syntax:
switchport vlan mac <mac_addr> vlan <vid>Argument | Description | |
Parameter |
| 48 bit unicast MAC address: xx:xx:xx:xx:xx:xx |
| VLAN ID required for the group to VLAN mapping. The range is from 1–4095. | |
Default | N.A | |
Mode | Port List Interface mode | |
Usage | Configure MAC address to VLAN ID association. To remove the MAC address to VLAN ID association, use the ‘no’ version of the command. | |
Example | Example: | |