3.18.2 LLDP Interface Configuration
Use this command to configure LLDP parameters for each port. Select the LLDP mode, enable CDP awareness, and configure whether an SNMP trap should be emitted when the LLDP neighbor table changes. Also, select optional TLVs (port description, system name, system description, capabilities, management address) to be included when LLDP information is transmitted.
Command Syntax:
lldp transmit
lldp receive
lldp cdp-aware
lldp trap
lldp tlv-select { management-address | port-description | system-capabilities | system-description | system-name }Argument | Description | |
Parameter |
| Enable/disable transmission of LLDP frames. |
| Enable/disable decoding of received LLDP frames. | |
| Configures if the interface shall be CDP aware (CDP discovery information is added to the LLDP neighbor table). | |
| Configures if an SNMP trap shall be emitted when the LLDP neighbor table changes for the interface. | |
| Enables/disables LLDP optional TLVs to transmit. | |
Default | N.A | |
Mode | Port List Interface mode | |
Usage | Enable LLDP system settings. To disable, use the ‘no’ version of the command. | |
Example | Example 1: Configure LLDP on port 1 as transmit only with CDP aware. | |