17.3.2 Alternate Functions of Port C
The Port C pins with alternate functions are shown in the table below:
| Port Pin | Alternate Function |
|---|---|
| PC6 |
RESET (Reset pin)
|
| PC5 |
ADC5 (ADC Input Channel 5)
|
| PC4 |
ADC4 (ADC Input Channel 4)
|
| PC3 |
ADC3 (ADC Input Channel 3)
|
| PC2 |
ADC2 (ADC Input Channel 2)
|
| PC1 |
SCK1 (SPI1 Master Clock output) |
| PC0 |
MISO1 |
The alternate pin configuration is as follows:
- RESET/PCINT14 – Port C, Bit 6
- RESET, Reset pin: When the RSTDISBL Fuse is programmed, this pin functions as a normal I/O pin, and the part will have to rely on Power-on Reset and Brown-out Reset as its reset sources. When the RSTDISBL Fuse is unprogrammed, the reset circuitry is connected to the pin, and the pin cannot be used as an I/O pin.
- PCINT14: Pin Change Interrupt source 14. The PC6 pin can serve as an external interrupt source.
If PC6 is used as a reset pin, DDC6, PORTC6 and PINC6 will all read 0.
- SCL0/ADC5/PCINT13 – Port C, Bit 5
- SCL0: Two-wire Serial Interface0 Clock. When the TWEN bit in TWCR0 is set (one) to enable the two-wire Serial Interface, pin PC5 is disconnected from the port and becomes the Serial Clock I/O pin for the two-wire Serial Interface0. In this mode, there is a spike filter on the pin to suppress spikes shorter than 50 ns on the input signal, and the pin is driven by an open drain driver with slew-rate limitation.
- PCINT13: Pin Change Interrupt source 13. The PC5 pin can serve as an external interrupt source.
-
PC5 can also be used as ADC input Channel 5. The ADC input channel 5 uses digital power.
- SDA0/ADC4/PCINT12 – Port C, Bit 4
- SDA0: Two-wire Serial Interface0 Data. When the TWEN bit in TWCR0 is set (one) to enable the two-wire Serial Interface, pin PC4 is disconnected from the port and becomes the Serial Data I/O pin for the two-wire Serial Interface0. In this mode, there is a spike filter on the pin to suppress spikes shorter than 50 ns on the input signal, and the pin is driven by an open drain driver with slew-rate limitation.
- PCINT12: Pin Change Interrupt source 12. The PC4 pin can serve as an external interrupt source.
- PC4 can also be used as ADC input Channel 4. The ADC input channel 4 uses digital power.
- ADC3/PCINT11 – Port C, Bit 3
- PC3 can also be used as ADC input Channel 3. The ADC input channel 3 uses analog power.
- PCINT11: Pin Change Interrupt source 11. The PC3 pin can serve as an external interrupt source.
- ADC2/PCINT10 – Port C, Bit 2
- PC2 can also be used as ADC input Channel 2. The ADC input channel 2 uses analog power.
- PCINT10: Pin Change Interrupt source 10. The PC2 pin can serve as an external interrupt source.
-
SCK1/ADC1/PCINT9 – Port C, Bit 1
- PC1 can also be used as ADC input Channel 1. The ADC input channel 1 uses analog power.
- SCK1: Master Clock output, Slave Clock input pin for SPI1 channel. When the SPI1 is enabled as a Slave, this pin is configured as an input regardless of the setting of DDB5. When the SPI1 is enabled as a Master, the data direction of this pin is controlled by DDC1. When the pin is forced by the SPI1 to be an input, the pull-up can still be controlled by the PORTC1 bit.
- PCINT9: Pin Change Interrupt source 9. The PC1 pin can serve as an external interrupt source.
- ADC0/MISO1/PCINT8 – Port C, Bit 0
- PC0 can also be used as ADC input Channel 0. The ADC input channel 0 uses analog power.
- MISO1: Master1 Data input, Slave Data output pin for SPI1 channel. When the SPI1 is enabled as a Master, this pin is configured as an input regardless of the setting of DDC0. When the SPI1 is enabled as a Slave, the data direction of this pin is controlled by DDC0. When the pin is forced by the SPI1 to be an input, the pull-up can still be controlled by the PORTC0 bit.
- PCINT8: Pin Change Interrupt source 8. The PC0 pin can serve as an external interrupt source.
The tables below relate the alternate functions of Port C to the overriding signals shown in Figure 17-5.
| Signal Name | PC6/RESET/PCINT14 | PC5/SCL0/ADC5/PCINT13 | PC4/SDA0/ADC4/PCINT12 |
|---|---|---|---|
| PUOE | RSTDISBL | TWEN0 | TWEN0 |
| PUOV | 1 | PORTC5 • PUD | PORTC4 • PUD |
| DDOE | RSTDISBL | TWEN0 | TWEN0 |
| DDOV | 0 | SCL_OUT0 | SDA_OUT0 |
| PVOE | 0 | TWEN0 | TWEN0 |
| PVOV | 0 | 0 | 0 |
| DIEOE | RSTDISBL + PCINT14 • PCIE1 | PCINT13 • PCIE1 + ADC5D | PCINT12 • PCIE1 + ADC4D |
| DIEOV | RSTDISBL | PCINT13 • PCIE1 | PCINT12 • PCIE1 |
| DI | PCINT14 INPUT | PCINT13 INPUT | PCINT12 INPUT |
| AIO | RESET INPUT | ADC5 INPUT / SCL0 INPUT | ADC4 INPUT / SDA INPUT0 |
| Signal Name | PC3/ADC3/ PCINT11 | PC2/ADC2/ PCINT10 | PC1/ADC1/SCK1/ PCINT9 | PC0/ADC0/MISO1/ PCINT8 |
|---|---|---|---|---|
| PUOE | 0 | 0 | SPE1 • MSTR | SPE1 • MSTR |
| PUOV | 0 | 0 | PORTC1 • PUD | PORTC0 • PUD |
| DDOE | 0 | 0 | SPE1 • MSTR | SPE1 • MSTR |
| DDOV | 0 | 0 | 0 | 0 |
| PVOE | 0 | 0 | SPE1 • MSTR | SPE1 • MSTR |
| PVOV | 0 | 0 | SCK1 OUTPUT | SPI1 SLAVE INPUT |
| DIEOE | PCINT11 • PCIE1 + ADC3D | PCINT10 • PCIE1 + ADC2D | PCINT9 • PCIE1 + ADC1D | PCINT8 • PCIE1 + ADC0D |
| DIEOV | PCINT11 • PCIE1 | PCINT10 • PCIE1 | PCINT9 • PCIE1 | PCINT8 • PCIE1 |
| DI | PCINT11 INPUT | PCINT10 INPUT |
PCINT9 INPUT |
PCINT8 INPUT |
| AIO | ADC3 INPUT | ADC2 INPUT | ADC1 INPUT | ADC0 INPUT |