6.9.5 LED
This user interface provides framework to add firmware files that will contain APIs to drive a LED. The LED and a series resistor needs to be connected to the GPIO pin as shown in the image below. The UI provides two options for the GPIO pin output drive - Active Low and Active High.

Follow these steps in order to configure and add this module to the project:
-
Click on the checkbox near the 'LED' module on the panel on the left hand side to enable this module to be added to the project
-
Select a GPIO pin and drive mode
Note:
Currently only one LED can be configured and added to the project.