21.4.7 Serial Data Reception
When the TPI physical layer is in receive mode, data reception is started as soon as a start bit has been detected. Each bit that follows the start bit will be sampled at the rising edge of the TPICLK and shifted into the shift register until the second stop bit has been received. When the complete frame is present in the shift register the received data will be available for the TPI access layer.
There are three possible exceptions in the receive mode: frame error, parity error and break detection. All these exceptions are signalized to the TPI access layer, which then enters the error state and puts the TPI physical layer into receive mode, waiting for a BREAK character.
- Frame Error Exception. The frame error exception indicates the state of the stop bit. The frame error exception is set if the stop bit was read as zero.
- Parity Error Exception. The parity of the data bits is calculated during the frame reception. After the frame is received completely, the result is compared with the parity bit of the frame. If the comparison fails the parity error exception is signalized.
- Break Detection Exception. The Break detection exception is given when a complete frame of all zeros has been received.