5.2.3.18 ZDO_StartNetworkConf_t Structure
Syntax
typedef struct
{
uint8_t activeChannel; //!< Current channel on which the device has connected.
ShortAddr_t shortAddr; //!< Assigned short address.
PanId_t PANId; //!< Received short network PANId.
uint64_t extPANId; //!< Received extended PANId if it was not determined during startup
ShortAddr_t parentAddr; //!< Parent short address
//Resulting status of a network start operation
//See StartNwkStatuses "details".*/
ZDO_Status_t status;
} ZDO_StartNetworkConf_t;Description
The ZDO_StartNetworkConf_t structure describes the parameters of the
ZDO_StartNetworkConf() function.