6.7 MCC Device Migration
Using an MCC configuration created for one device on a different device is called MCC device migration.
It is possible that attempting to use an MCC configuration on a device other than the one for which it was created might appear not to fail. It is entirely the user's responsibility to determine if the MCC code generated as the result of device migration is suitable for use in their application.
Unintended MCC device migration may occur if the selected device in the MPLAB X IDE
project is changed after MCC has been configured for that project. Copying an MCC
configuration file (*.mc3) to another MPLAB X IDE project may also
cause MCC device migration or other unintended operations.