Appendix A.1 - Reading Serial Number Using
AT Command
To read the Serial Number from the DUT, use the AT+ECCRDSER command. The
following figure illustrates sample output. For more details about the syntax of the AT
command and the expected output, refer to the AT
Commands.Figure . Reading Serial Number
Note: Serial number (Common Name) is prefixed with
sn, therefore serial number becomes
sn0123C7E756AF138601.