37.2.4.3.1 Transition Bit (T-Bit)
Unlike I2C, where the ninth data bit represents ACK/NACK, the ninth data bit in an I3C SDR Data Word is a Transition Bit (T-bit).
When the Controller is writing data to the Target, the ninth data bit (T-bit) of each SDR
Data Word is a Parity bit calculated using odd parity, which is helpful in detecting
noise-caused errors on the bus. The value of this Parity bit is the XOR of each of the
eight data bits with ‘1’. Figure 37-13 shows an example Write Data Word from the Controller with the Parity T-bit
included.
0x96)0’. To continue the message, the Target
returns the ninth T-Bit as ‘1’ and monitors the SDA line. If the SDA
line remains high on the next falling SCL edge, the Target continues to send the next
data value. If the SDA line is low on the next falling SCL edge (Restart), then the
Controller has aborted the data transfer and the Target module does not send the next
data. This condition can be monitored using the RSCIF flag.Figure 37-14 shows an example Read Data Word from the Target where the End-of-Data bit is asserted by the Target. Figure 37-15 shows an example Read Data Word from the Target where the Controller aborts the transaction by asserting the End-of-Data bit.
1, the user must write the next byte to
I3CxTXB Transmit Buffer before the Transmit FIFO becomes empty. The Target module
responds with an End-of-Data T-bit = 0 as soon as the Transmit FIFO
becomes empty. This applies to Private Read Transactions and while sending the IBI Payload. 0x96 and 0xD4)0x96 and 0xD4)