37.2.9 In-Band Interrupt (IBI)
The MIPI I3C® Specification allows the I3C devices on the bus to generate an In-Band Interrupt (IBI) for the Active Controller to service using the SDA and SCL lines. This makes it possible for the devices on the bus to generate interrupts without using any external interrupt lines.
Each device on the I3C bus has a priority level encoded into its Controller-assigned
Dynamic address, where addresses with lower numeric values have higher priority levels.
This is a natural outcome of the I3C Address Arbitration,
where address bits with value ‘0’ are prioritized over bits with value
‘1’. This means that when multiple devices request IBI at the same
time, devices with lower numeric value addresses (and subsequently higher priority
levels) will have their IBI requests processed sooner than devices with higher numeric
value addresses.
1). This is communicated to
the Controller during the Dynamic Address Assignment procedure or when the Controller
requests for it using the GETBCR (Get Bus Characteristics Register) Direct Common Command
Code (CCC).- The Target has a Dynamic Address assigned
- IBI is enabled on the bus by the
Controller (IBIEN =
1)
The Target can request for an In-Band Interrupt by setting the IBIREQ bit. Once the
IBIREQ bit is set, the Target waits for the Bus Available condition and
then issues a Start on the bus by pulling the SDA line low (standard IBI). The Active
Controller acknowledges the Start condition by sending clocks on the SCL
line(1) marking the beginning of the Arbitrable Address Header, during which the Target transmits its Dynamic
Address in Read mode (R/W bit = 1) on the
bus.
However, the Target does not always need to wait for the Bus Available condition to occur on the bus. If another device on the bus issues a Start signal before the Bus Available condition occurs, the Target participates in the Address Arbitration by transmitting its Dynamic Address on the bus (passive IBI).
- If the Controller does not acknowledge the Start condition issued by the Target, the Bus Time-out feature can be used to abort the Hot-Join or In-Band Interrupt request.
- It is recommended to check the
value of IBIEN bit in the I3CxEC Events
Command register before requesting an In-Band Interrupt. The Controller can
enable/disable In-Band Interrupt (ENINT/DISINT) globally on the bus by
broadcasting the ENEC/DISEC CCC (Enable/Disable Target Events Command), which is
reflected in the I3CxEC register. If the IBIREQ bit is set when IBIEN =
0, the Target module will begin the IBI process as soon as the Controller enables In-Band Interrupt and IBIEN bit is set by the hardware.
- When an In-Band Interrupt is
requested in Static Address SDR mode (SASDRMD =
1), the Target sends its Static Address on the bus for arbitration if a Dynamic Address has not been assigned. If the Target has a Dynamic Address assigned, then the Dynamic Address will be sent on the bus for arbitration. - It is possible that the Target
loses arbitration while requesting an IBI when the Controller attempts to write
to the Target at the same time. The Controller drives the bus with the Target’s
address with R/W =
0(write, for private write transaction), whereas the Target drives the bus with its own address with R/W =1(read, for IBI request). When this happens, the Target loses the arbitration and proceeds forward with the private write transaction with the Controller as described in Private Transaction.
The IBI process that the Target follows is described in Figure 37-44.