37.2.7.2.4 Set New Dynamic Address (SETNEWDA)
The Controller uses the Direct SETNEWDA CCC to set a new Dynamic Address for the Target when the Target already has a Dynamic Address assigned. The frame format for Direct Write SETNEWDA CCC is shown in Figure 37-27. The Target’s new Dynamic Address is the first 7 bits of the 9-bit Dynamic Address field. This new address is stored in the I3CxDADR register. Refer to Changing Dynamic Address for more details.