5.4.4.3 Write Remote Characteristic Value for Multiple Links(CHWM,<hex16>,…)
Format:
CHWM,<hex16>,<hex16>,<hex value>
Command CHWM writes the content of the GATT service characteristic to the
dedicated remote device by connection handle for multiple links.
This command takes three parameters. The first parameter is the 16-bit hex value of the
connection handle, and the second parameter is the 16-bit hex value of the handle
corresponding to the characteristic of the GATT service. The user must find a match between
the handle and its characteristic UUID by using command LCM. The third
parameter is the content to be written to the characteristic.
- An active connection with a peer device exists.
- The command
CIstarts the client operation. - The handle parameter is valid and the corresponding characteristic is writable according to its property.
The content value is written to the remote peer device. The writing method depends on the property of the characteristic.
- Value 0x0001 (01 00 over the air in little-endian) – Starts the notification
- Value 0x0002 (02 00 over the air in little-endian) – Starts the indication
- Value 0x0000 – Stops both notification and indication
| Example: | CHWM,0071,001A,64
|
// Set the value of the characteristic with the value handle 0x001A to 0x64 on the remote device |
CHWM,0071,001B,0100 |
// Set connection handle value 0x0071 // Start notification on characteristic by writing 0x0001 to its configuration handle 0x001B on remote device | |
| Response: | AOK
| // Success |
Err |
// Syntax error, invalid parameter, not connected or characteristic not writable |