5.4.4.6 List Remote Services for Specific Link (LCM…)
Format:
LCM,<hex16>[,<P,UUID>]
The LCM command is a multi-link version of the LC
command. The LCM command has a first mandatory parameter that indicates
the connection handle for a specific connection. The following parameters are the same
with the LC command as well as the usage.
| Example: | LCM,0071
| // List all client services over the 0x71 connection handle |