5.6 Device Test Mode (DTM)
The RNBD451 module has support for a special mode
called Device Test Mode (DTM). By using the DTM command, the user can
configure the RNBD451 module to operate in the
DTM. Staying in the DTM mode, the RNBD451 module
supports a series of DTM commands. In the DTM mode, all the input commands and response
events are in HCI format. The first byte of HCI format is a packet type, where 0x01
represents the command packet and 0x04 represents the event packet. The RNBD451 module supports seven HCI commands. The
following section describes each HCI command in detail. If users send the software reset
command, the RNBD451 module resets and enters
into Data mode.