5.4.3.10 Customized Multiple Services
If there is a need for customized multiple services, perform the following steps:
- Use command
PZto clear any previously defined services. - Use command
PSto set the UUID for the first service. - Use one or more command
PCto add one characteristic at a time to the first service. - Use command
PSto set the UUID for another service. - Use one or more command
PCto add one characteristic at a time to the service. - (If necessary) Repeat step 4 and step 5 to define more services.