9 Appendix: Programming the Device Using FlashPro Express
(Ask a Question)This section describes how to program the PolarFire device with the programming job file using FlashPro Express. The job file is available at the following design files folder location: mpf_an5341_v2024p1_df\Programming_Job.
To program the device, perform the following steps:
- On the host PC, launch the FlashPro Express software.
- Click New or select New Job Project from FlashPro Express Job from Project menu to create a new job project, as shown in the following figure.
Figure 9-1. FlashPro Express Job Project - Enter the following in the New Job Project from FlashPro Express Job dialog box:
- Programming job file: Click Browse and navigate to the location where the job file is located and select the file. The default location is: <download_folder>\mpf_an5341_v2024p1_df\Programming_Job.
- FlashPro Express job project location: Click Browse and navigate to the FlashPro Express project location.
Figure 9-2. New Job Project from FlashPro Express Job - Click OK. The required programming file is selected and ready to be programmed in the device.
- The FlashPro Express window appears as shown in the following figure. Confirm that a programmer number appears in the Programmer field. If not, confirm the board connections and click Refresh/Rescan Programmers.
Figure 9-3. Programming the Device - Click RUN. When the device is programmed successfully, a RUN PASSED status is displayed as shown in the following figure.
Figure 9-4. FlashPro Express—RUN PASSED - Close FlashPro Express or click Exit in the Project tab.