12 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the most current publication.

Table 12-1. Revision History
RevisionDateDescription
A06/2024The following is the list of changes in revision A of the document:
  • The document was migrated to the Microchip template.
  • The document number was updated from 50200755 to DS00005341.
  • The document ID was updated from DG0755 to AN5341.
  • Updated the document for Libero® v2024.1.
13.0—The following is a summary of the changes made in this revision.
  • Updated the document for Libero SoC v2022.1.
  • Removed information related to Splash kit.
12.0—

The following is a summary of the changes made in this revision.

11.0—

Added Appendix B: Running the Tcl Script.

10.0—

The following is a summary of the changes made in this revision.

  • Updated the document for Libero SoC v12.2.
  • Removed the references to Libero version numbers.
9.0—Updated the document for Libero SoC v12.0.
8.0—The following is a summary of the changes made in this revision.
  • Updated the document for Evaluation and Splash kit.
  • Updated the document for Libero SoC PolarFire v2.3.
7.0—The document was updated for Libero SoC PolarFire v2.2.
6.0—The document was updated for Libero SoC PolarFire v2.1.
5.0—The following is a summary of the changes made in this revision.
  • The document was updated to include IP core.
  • Design Requirements was edited to add CORERESET_PF details and, JESD204B Interface Design, was updated with CORERESET_PF IP core.
4.0—The following is a summary of the changes made in this revision.
  • The document is updated to include features and enhancements introduced in the Libero SoC PolarFire v2.0 release.
  • Updated the GUI screens and COM port details with respect to the Libero SoC PolarFire v2.0 release.
3.0—The following is a summary of the changes made in this revision.
  • The document was updated to include features and enhancements introduced in the Libero SoC PolarFire v1.1 SP1 release.
  • Information about resource utilization was updated.
  • List of reference was added. For more information, see Appendix 3: References.
2.0—The following is a summary of the changes in this revision.
  • The document was updated for Libero SoC PolarFire v1.1 release.
  • Information about resource utilization was added.
1.0—Initial release.