7 Setting Up the Demo
(Ask a Question)Important: To run the Libero design using TCL script, see Appendix B: Running the Tcl Script.
After generating the bit stream, the PolarFire device must be programmed. To program the PolarFire device on Evaluation kit, perform the following steps:
- Ensure that the jumper settings on the board are same as listed in the following table.
Table 7-1. Jumper Settings Jumper Description J18, J19, J20, J21, J22 Close pin 2 and 3 for programming the PolarFire FPGA through FTDI J28 Close pin 1 and 2 for programming through the on-board FlashPro5 J26 Close pin 1 and 2 for programming through the FTDI SPI J27 Close pin 1 and 2 for programming through the FTDI SPI J4 Close pin 1 and 2 for manual power switching using SW3 J12 Close pin 3 and 4 for 2.5 V - Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the host PC to the J5 (FTDI port) on the board.
- Power on the board using the SW3 slide switch.
- For external loopback demo, connect TXN to RXN and TXP to RXP using the 2 SMA to SMA cables as shown in the following figure.The following figure shows the board setup for external loopback demo.
Figure 7-1. Board Setup (Evaluation Kit) When the board is powered up, power supply LEDs DS3 to DS14 glow. For more information about LEDs on the PolarFire Evaluation Board, see UG0747: PolarFire FPGA Evaluation Kit User Guide.
Important: For PCB loopback demo, SMA cables are not required. User can skip Step 5. - Double-click Run PROGRAM Action from the Libero > Design Flow tab.
- Right-click Run Program Action and select View Report to view the corresponding log file in the Reports tab.
When the device is successfully programmed, a green tick mark appears as shown in the following figure.
After programming the device, see Running the Demo to run the JESD204B stand-alone demo.