4 Simulating the PolarFire JESD204B Design
(Ask a Question)Before you begin:
- Start Libero SoC and select Project -> Tool Profiles.
- In the Tool Profiles window, select Synthesis and Simulation on the Tools panes and select the latest active installation directory paths for these two tools.
For Simulation, browse the design files folder, create Libero Project using provided TCL scripts, and click Simulate as shown in Figure 4-1. See Appendix B: Running the Tcl Script.
A testbench is provided to simulate the JESD204B PRBS pattern and waveform selection. Figure 4-2 shows the interaction between testbench and the design.
The testbench generates the test selection for the PRBS input (PRBS7, PRBS15, PRBS23, and PRBS31) and waveform input (sine wave, sawtooth wave, triangle wave, and square wave). It also monitors the JESD204B output status signals (SYNC_N, ALIGNED, and CGS_ERR) for the verification of JESD204B phases, and PRBS checker output status signals O_BAD and O_ERROR[4:0].
The following table lists the simulation signals.
| Signal | Description |
|---|---|
| Input Signals | |
| P_W_SEL | Input to select the PRBS pattern or waveform |
| WAVE_SEL[1:0] | Input to select the type of waveform |
| PRBS_SEL[1:0] | Input to select the type of PRBS pattern |
| ERR_EN | Input to enable error in the PRBS pattern |
| NSYSRESET | Active low reset signal |
| SYSCLK | 156.25 MHz generated clock for external loopback design. 125 MHz generated clock for internal loopback design. |
| Output Signals | |
| TB_DATA_OUT | Output data from CoreJESD204BRX |
| TB_RX_SOMF | SOMF_0[3:0] signal received from the CoreJESD204BRX block |
| TB_RX_SOF | SOF_0[3:0] signal received from the CoreJESD204BRX block |
| TB_SYNC_N | SYNC_N signal, which indicates the link status |
| TB_ALIGNED | ALIGNED signal, which indicates that all transceiver lanes are aligned |
| TB_LINK_CD_ERR | LINK_CD_ERR[0] signal, which indicates a link configuration data mismatch error |
| TB_UCC_ERR | UCC_ERR[0] signal, which indicates an unexpected control character error |
| TB_NIT_ERR | NIT_ERR[3:0] signal, which indicates the “not in table” error. This signal is controlled by LANE0_RX_CODE_VIOLATION[3:0] |
| TB_DISP_ERR | DISP_ERR[3:0] signal which indicates the disparity error. This signal is controlled by LANE0_RX_DISPARITY_VIOLATION[3:0] |
| TB_CGS_ERR | CGS_ERR signal, which indicates the code group synchronization error. This signal is controlled by the CGS_ERR[0] signal. |
| TB_RX_READY | LANE0_RX_READY signal received from the transceiver block |
| TB_0_BAD | Error flag |
| TB_O_ERROR[4:0] | Number of errors occurred during PRBS check |
To run the simulation, go to Stimulus Hierarchy and verify if PF_JESD204B_SA_TOP_TB_8b file is set as active stimulus. If not set, right-click on the file and select Set as active stimulus.
When the simulation is initiated, ModelSim compiles all the design source files, runs the simulation, and configures the waveform viewer to show the simulation signals.