2.9.3.2 RX AMI Model
(Ask a Question)SerDes supports the programmable single pole continuous time linear equalization (CTLE) at the receiver. The linear equalization comprises of amplifying higher frequency components that have been more severely attenuated by the Interconnect, or attenuating the lower frequency components to a greater degree than the higher frequency components.
The low-frequency attenuation level and the low-frequency flat-band bandwidth are programmable, as shown in the following figure.
Both ALF and ωc (f0) can be set to maximize the signal quality of the receiver for achieving the highest possible bit error rate (BER).
- Alf: Low-frequency dB loss of the filter. The range is from 0 to 50, default value is 6.
- f0: High pass cut-off frequency. The range is from 1e6 to 5e10, default value is 1e9.