2.3.3.2 SerDes I/O Power (SERDES_x_VDDAIO)
(Ask a Question)The target impedance of the SERDES_x_VDDAIO pin is calculated as 240 mΩ, based on the following values (see Power Supply):
- VSUPPLY = 1.2 V
- Itrans= 250 mA
Ripple = 5%
The following figure shows the impedance of the plane (SERDES_x_VDDAIO) improved by the decoupling capacitors. The impedance of the plane is kept under 0.2 Ω till 100 MHz.