2.2.2 Plane Layout
(Ask a Question)Use the VDD plane, as shown in the following figure.
Important: The plane can be routed in
multiple ways to have dedicated and low-impedance plane.

Use the VDD plane, as shown in the following figure.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.