1.5.3.14 SYS_WIFIPROV_Tasks Function

C

uint8_t SYS_WIFIPROV_Tasks ( SYS_MODULE_OBJ object)

Summary

Maintains the Wi-Fi Provisioning System tasks and functionalities.

Description

This function is used to run the various tasks and functionalities of Wi-Fi Provisioning system service.

Precondition

The SYS_WIFIPROV_Initialize function should have been called before calling this function.

Parameters

ParamDescription
objectSYS WIFI Provisioning object handle, returned from SYS_WIFIPROV_Initialize

Returns

return SYS_WIFIPROV_STATUS if client provided object is valid, else return SYS_WIFIPROV_OBJ_INVALID.

Example

if (SYS_WIFIPROV_OBJ_INVALID != SYS_WIFIPROV_Tasks (wifiProvServHandle))
{
    
}

Remarks

None