1.3.3.25 SYS_NET_Close Function
C
void SYS_NET_Close ( SYS_MODULE_OBJ object )
Summary
Deinitializes the specific instance of the NET System service
Description
This function deinitializes the specific module instance disabling its operation. Resets all of the internal data structures and fields for the specified instance to the default settings.
Precondition
The SYS_NET_Open function should have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| object | SYS NET object handle, returned from SYS_NET_Open |
Returns
None.
Example
// Handle "objSysNet" value must have been returned from SYS_NET_Open. SYS_NET_Close (objSysNet);
Remarks
Once the Open operation has been called, the Close operation must be called before the Open operation can be called again.