1.3.3.29 SYS_NET_SendMsg Function
C
int32_t SYS_NET_SendMsg(SYS_MODULE_OBJ obj, uint8_t *buffer, uint16_t len)Summary
Returns No of Bytes sent to peer using the System NET instance.
Description
This function returns the number of bytes transmitted to the peer.
Precondition
SYS_NET_Open should have been called.
Parameters
object - SYS NET object handle, returned from SYS_NET_Open data - valid data buffer pointer len - length of the data to be transmitted
Returns
SYS_NET_SERVICE_DOWN - Indicates that the System NET instance is not connected to the peer
SYS_NET_PUT_NOT_READY - Indicates that the System NET instance Put is NOT ready
SYS_NET_PUT_BUFFER_NOT_ENOUGH - Indicates that the System NET instance cannot transmit as the available buffer is less than the bytes to be transmitted
Positive Non-Zero - Indicates the number of bytes transmitted to the peer
Example
// Handle "objSysNet" value must have been returned from SYS_NET_Open. while(SYS_NET_SendMsg(objSysNet, "hello", 5) <= 0);
Remarks
None.